Communication Setup editor
How do I access the Communication Setup editor?
From the
Explorer
, under the FactoryTalk Linx
data server, double-click Communication Setup
.The
Communication Setup
editor is to create and modify FactoryTalk Linx
configurations.Use the
Communication Setup
editor to:- Add drivers
- Add devices
- Set up driver and device properties
- Set up device shortcuts in aFactoryTalk Linxconfiguration
Provide Feedback