FactoryTalk Linx Help
FactoryTalk® Linx
is a FactoryTalk®
Live Data server and
communications service designed to deliver control system information from Allen-Bradley®
control products to the Rockwell Automation®
FactoryTalk®
software portfolio and Studio 5000®
design software. While FactoryTalk Linx
can communicate with most Allen-Bradley
Programmable Logic Controllers (PLC®) and many other control
products, it is optimized to work with Logix 5000™
Programmable
Automation Controllers (PAC) and the PlantPAx®
process controller
using EtherNet/IP. It gives the fastest data rates and capacity possible while minimizing
the impact on automation networks and control system operation. Use FactoryTalk Linx to:- Browse devices in the network - The network browser provides the ability to discover devices in an automation system, permit the user to navigate the topology, perform device commissioning, access device properties, and diagnostic statistics.
- Acquire data -FactoryTalk Linxprovides a scalable solution that can support small applications running on a single computer with a single controller, to large distributed and even redundant data server configurations communicating with many controllers.
- Use theFactoryTalk® Linx™ GatewayRemote Proxy Server - Remote Devices via Proxy Service allows FactoryTalk Linx on one computer to bridge through a central FactoryTalk Linx Gateway Professional workstation on the network to communicate with automation system devices on a different network.
TIP:
Prior to version 6.00
FactoryTalk Linx
was called RSLinx Enterprise
. Because of this, some portions of the software installation and documentation still
contain references to the previous RSLinx Enterprise
name.Provide Feedback