Backup and restore FactoryTalk Linx configuration

Starting with v6.21, the
FactoryTalk Linx
shortcut and driver configurations can be backed up and restored in
FactoryTalk Administration Console
. It is important to create a backup of the system configuration after any significant changes are made, to aid in recovering system operation should a computer hardware or operating system failure occur.
The
FactoryTalk Linx
configurations can be backed up and restored from the
FactoryTalk Administration Console
. The
FactoryTalk Linx
configuration is contained in four areas that must all be retained if you plan to restore the system later. The application contains the server and shortcut configuration,
FactoryTalk Linx
stores driver information needed by the shortcuts separately, the FactoryTalk System folder contains the security policy settings utilized by
FactoryTalk Linx
and
FactoryTalk Policy Manager
maintains the CIP Security configuration used by
FactoryTalk Linx
when CIP Security is enabled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal