FactoryTalk Linx features
FactoryTalk Linx version 5.90.00 and earlier:
- Is delivered and installed with theFactoryTalk Services Platformwhich is included with mostRockwell Automationsoftware products.FactoryTalk Linxis also delivered within thePanelView PlusElectronic Operator Interface (EOI) terminal’s firmware.TIP:TheFactoryTalk Services PlatformInstallation includes several useful tools. UseFactoryTalk Live Data Test Clientto interface withFactoryTalk Linxto read and write data directly to controllers. For more information aboutFactoryTalk Live Data Test Client, seeFactoryTalk Services PlatformOnline Help.
- Is accessed as an embedded component within each software package that uses its services. ConfigureFactoryTalk Linxusing theCommunication Setupeditor launched from aFactoryTalkapplication design environment (for example, FactoryTalk® View Studio) or from theFactoryTalk® Administration Console.
- Provides access to controller and device data from anyFactoryTalkapplication usingFactoryTalk Live Data.
- Is highly optimized forLogix 5000communications.
- Starting with version 5.30.00, supportsFactoryTalk® Alarms and Events. For more information aboutFactoryTalk Alarms and Events, See.FactoryTalk Alarms and EventsOnline Help
- Starting with version 5.30.00, network applications provide the option of specifying a secondary, or redundant, server to take over when the primary server fails.
- Starting with version 5.60.00, reads data directly from devices using parameters specified in the device’s Electronic Data Sheet (EDS) file.
- Starting with version 5.70.00, receives data fromLogix 5000controllers directly via the unsolicited message.
- Starting with version 5.70.00, is able to communicate withMicro800™controllers.
- Starting with version 5.80.00, reads energy usage information from devices that support theODVA™CIP™Energy object.
- Starting with version 5.90.00, readsLogix 5000tag-extended properties (for example,@Min,@Max,@Description) and delivers them to FactoryTalk View applications. WithFactoryTalk Linxversion 6.10.00, this capability is enhanced to improve read performance and adds the ability to provide a description using information indirectly associated with a tag. This enables a FactoryTalk View SE client to obtain descriptions for tag elements that do not directly have a description assigned. This is similar to the description of pass-through capability ofStudio 5000 Logix Designer.
- Starting with version 5.90.00, removesLogix 5000tag requests when their external access is switched tono accessin Logix Designer, and the tags can be removed from the controller while it is operating.
- Starting with version 5.90.00, permits communications to specificLogix 5000shortcuts to be inhibited to reduce the impact ofLogix 5000controllers that are disabled or offline.
FactoryTalk Linx version 6.00.00:
- Starting with version 6.00.00, EtherNet/IP network drivers can be configured directly from theFactoryTalk LinxNetwork Browser control embedded withinStudio 5000and other Rockwell Automation design software.
- Starting with version 6.00.00, provides access toLogix 5000tag-based alarm attributes (for example,@Alarm…).
- Offers a variety of communication drivers and routing options.
- Supports Local applications (also called standalone applications) for smaller systems, and Network applications (also called distributed applications) for larger systems.
- Starting with version 6.00.00, enables the configuration of two redundant shortcut paths to a singleLogix 5000controller to support high availability systems that desire to retain communications when a path through a network becomes disabled.
- Starting with version 6.00.00, permits the configuration of two shortcut paths to the primary and secondaryLogix 5000controllers in a redundantControlLogixrevision 31.5x system to retain communications when a redundancy switchover occurs.
- FactoryTalk Linx6.00.00 added the ability to provide communications and browsing services for Studio 5000 andControlFLASH.FactoryTalk Linxversion 6.10.00 extends this functionality to support theConnected Components Workbench(CCW) version 12.00.00 andFactoryTalk AssetCentreversion 9.00.00.
- FactoryTalk Linxversion 6.00.00 updated both the Virtual Backplane and USB drivers and had them signed by Microsoft to permit them to operate on a workstation with Windows 10 Secure boot enabled.FactoryTalk Linxversion 6.10.00 extends this functionality to include the drivers associated with the 1784-PCICS and 1784-PCKTS cards. InFactoryTalk Linxversion 6.20.00, the 1784-PKTX driver is signed by Microsoft to support Windows 10 secure boot.
FactoryTalk Linx version 6.10.00:
- FactoryTalk Linxversion 6.10.00 added a new standalone version ofFactoryTalk LinxNetwork Browser that can be launched from the Windows Start Menu. Previously this component was only available from within otherRockwell Automationsoftware (for example.ControlFLASHandStudio 5000 Logix Designer). The Network Browser can be used to visualize the network to determine which devices are active in the system.
- FactoryTalk Linxversion 6.10.00 added FactoryTalk Security Product Policy to provide more control over the configuration for authorized users.
- FactoryTalk Linxversion 6.10.00 added logging of FactoryTalk Audit messages to track configuration changes ofFactoryTalk Linx.
- FactoryTalk Linxversion 6.10.00 supports a new capability in Logix5000 V32 controllers to change the names of tags and structure members on a running controller. WhenFactoryTalk Linxdetects the rename operation, it will immediately stop requesting the old names and provide an appropriate error status back to theFactoryTalksoftware that requested the data, making it easier to locate other software that is impacted by the rename operation.
- FactoryTalk Linxversion 6.10.00 added the ability to receive unsolicited messages using PLC-2 Unprotected Writes. This enables Logix5000 or legacy controllers to send information to a FactoryTalk software package usingFactoryTalk Linx.
- FactoryTalk Linxversion 6.10.00 changes the default setting for the “listen on EtherNet/IP Encapsulation port” (port 44818) for its Ethernet driver so thatFactoryTalk Linxwill respond to network browse requests and receive unsolicited messages from Logix5000 controllers.RSLinx Classicversion 4.00.01 or earlier allocated this port by default but was updated with version 4.10.00 to not allocate the port to reduce the likelihood of a conflict between these two software packages.
- FactoryTalk Linxversion 6.10.00 added the ability to configure two independent instances of the data service on a single Windows operation system. It allows applications to have more tags, data clients (for example, HMI clients), and/or controllers without affecting the otherFactoryTalk Linxdata server.
FactoryTalk Linx version 6.11.00:
- FactoryTalk Linxversion 6.11.00 added the ability to establish secure encrypted communications with FactoryTalk Policy Manager using CIP security. Seefor more information about CIP security.FactoryTalk Policy ManagerOnline Help
FactoryTalk Linx version 6.20.00:
- FactoryTalk Linxversion 6.20.00 added the ability to access information inside of devices that support the Open Device Vendors Association (ODVA) Common Industrial Protocol (CIP), using the Class, Instance and Attribute (CIA) messaging with theCIP Object - Class/Instance/Attribute Messageshortcut type.
- TheFactoryTalk SecurityPolicy forFactoryTalk Linxwas enhanced to control the user’s capabilities from theFactoryTalk LinxNetwork Browser and to control access to CIA Messaging.
- In conjunction withFactoryTalk Linx Gateway, provides standard OPC connectivity into the FactoryTalk system for third-party products. For more information aboutFactoryTalk Linx Gateway, refer to theFactoryTalk Linx GatewayHelp.FactoryTalk Linxversion 6.20.00 adds the ability to access information inside of devices that support the Open Device Vendors Association (ODVA) Common Industrial Protocol (CIP), using the Class, Instance and Attribute (CIA) messaging with theCIP Object - Class/Instance/Attribute Messageshortcut type.
- Starting with version 6.20.00,FactoryTalk Linxsupports tag communication with data types as LINT, ULINT, LREAL, USINT, UINT, and UDINT.
- Starting with version 6.20.00,FactoryTalk Linxinstance02 supports Logix-based Alarms and Events.
- Starting with version 6.20.00,FactoryTalk Linxprovides the ability to communicate using solicited messaging withAllen-Bradleycontrollers using PLC-5 or SLC-5 messaging over theDH+network without having a 1784-PKTX card installed on the computer. This is achieved by using the 1756 EtherNet/IP module bridging across aControlLogixchassis to aDH+network connected to a 1756-DHRIO module.
- FactoryTalk Linxversion 6.20.00 adds the ability to configure existing drivers inFactoryTalk LinxBrowser >Configure Driversdialog box.
- FactoryTalk Linxversion 6.20.00 adds the ability to view new CIP Identity Object Manufacturer information, which includesCatalog Number,Manufacture Date,Hardware Revision,Warranty, andSeries.
- FactoryTalk Linxversion 6.20.00 adds FactoryTalk Audit information to diagnose configuration changes made from theFactoryTalk LinxNetwork Browser.
- FactoryTalk Linxversion 6.20.00 adds the ability forFactoryTalk LinxNetwork Browser to browse through the 5094 IO HART modules and display HART connected devices in the topology.
- FactoryTalk Linxversion 6.20.00 adds the ability for theFactoryTalk LinxNetwork Browser to access Device Statistics to help diagnose devices.
- FactoryTalk Linxversion 6.20.00 adds the ability for theFactoryTalk LinxNetwork Browser to access Device Configuration to help configure the port and network configuration of a device.
- FactoryTalk Linxversion 6.20.00 adds the ability for theFactoryTalk LinxNetwork Browser to launch an Internet browser to open the device-embedded webpage.
- FactoryTalk Linxversion 6.20.00 provides the ability forFactoryTalkandPanelView PlusV12 terminals to access the four attributes @Name, @Quality, @Timestamp, and @Scope.
- FactoryTalk Linxversion 6.20.00 adds the ability forFactoryTalkandPanelView PlusV12 terminals to access PlantPAX Controller extended tag properties: @Library, @Instruction, @Label, @Area, @URL, and @Navigation.
- Starting from version 6.20.00,FactoryTalk Linxchanged to use a device’sNetwork Pathto store the location of the device in a system, which enables the user to configure and store the shortcut path using the device's IP address and slot number in a chassis.
- FactoryTalk Linxversion 6.20.00 provides the Chinese, German, French, and Japanese localized user interface (the localizedFactoryTalk Linxcan only be installed when installing the same localized version ofFactoryTalk View SE).
- FactoryTalk Linxversion 6.20.00 adds the ability to close unused connections after a specified time.
- FactoryTalk Linxversion 6.20.00 adds the ability to specify the max number of connections for aProcessorshortcut connecting to PLC/SLC controllers using the DHRIO module.
FactoryTalk Linx version 6.21.00:
- FactoryTalk Linxversion 6.21.00 adds anAboutdialog box inFactoryTalk LinxNetwork Browser to show the version of the installedFactoryTalk LinxNetwork Browser andFactoryTalk Linx, or to view the copyright and contact information.
- FactoryTalk Linxversion 6.21.00 adds the ability to detect devices that support a user initiating LED blink operation and presents an option on the device property dialog to locate where a device is physically installed by flashing a device's LEDs.
- FactoryTalk Linxversion 6.21.00 adds an option to set theTerminal file transfer communication package size. Users can choose either 2000 bytes or 1400 bytes for the terminal communication package size (Default 2000). The smaller packet size improves the transfer time when FactoryTalk View Studio ME is operating within a virtual machine.
- FactoryTalk Linxversion 6.21.00 adds two predefined tags (@NamespaceTimestamp, @NamespaceTimestampOPC) to show a time stamp for the last Logix controller namespace change.
- FactoryTalk Linxversion 6.21.00 included a new tool named, which enables theFactoryTalk LinxConfiguration Import Export ToolFactoryTalk Linxdriver and shortcut configuration to be extracted, modified, and replaced, providing an alternative to manually creating or editing the driver and shortcuts configuration from theFactoryTalk Administration Consoleuser interface.
- FactoryTalk Linxversion 6.21 supports to backup and restore shortcut and driver configurations inFactoryTalk Administration Console.
- FactoryTalk Linxversion 6.21 adds the ability to generate SysLog for select events including CIP Security configuration changes, network configuration changes, andFactoryTalk Linxservice restart.
- FactoryTalk Linxversion 6.21.00 improved performance for design software that usesFactoryTalk Linxfor communications direct to devices (for example,Studio 5000 Logix DesignerandControlFLASH Plus).
- InFactoryTalk Linxversion 6.21.00, theFactoryTalk LinxRedundancy Module Configuration Tool can be launched from theFactoryTalk LinxNetwork browser.
FactoryTalk Linx version 6.30.00:
- FactoryTalk Linxversion 6.30.00 adds an option to enable or disable CIP Security (Port 2221) for the server workstation or a device via theNetwork Browser.
- FactoryTalk Linxversion 6.30.00 supports browsing 5015 adapters and optimizes the user interface of 5015 adapters with their I/O modules.
- FactoryTalk LinxNetwork Browserversion 6.30.00 supports indicating the offline status of devices.
- FactoryTalk Linxversion 6.30.00 adds one predefined tag (@TrackedStateValue) to show the tracked state change detection value from a Logix L7 series controller.
- FactoryTalk Linxversion 6.30.00 adds anLLDPtab in theNetwork Browserto view and edit the Link Layer Discovery Protocol (LLDP) detection status of a device.
- FactoryTalk Linxversion 6.30.00 adds@RedundancyEnabledand@RedundancyStatepredefined tags associated with a processor shortcut, to indicate if the associated controller is operating in a ControlLogix Redundancy configuration and its current operational state. These tags are helpful for Human Machine Interface (HMI) displays that monitor the operation of a redundant ControlLogix controller’s operation.
- FactoryTalk LinxNetwork Browserversion 6.30.00 supports browsing of GuardLink connected devices.
- FactoryTalk Linxversion 6.30.00 removes the "IO Linx" communications driver.
- FactoryTalk Linxversion 6.30.00 enhances the configuration of port 44818 that keeps the same configuration status in bothFactoryTalk LinxandFactoryTalk Administration Console.
- FactoryTalk Live Dataversion 6.30.00 extends the supported subscription rates to include 600, 700, 800, and 900 ms.
- FactoryTalk Live Dataversion 6.30.00 adds leading zeros for array indexes so thatFactoryTalk Live DataTag browser sorts array elements in the proper numerical order.
- FactoryTalk Linxversion 6.30.00 raises the minimum DCOM authentication level to Packet Integrity. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
FactoryTalk Linx version 6.31.00:
- FactoryTalk Linxversion 6.31.00 supports adding and configuring unsolicited message shortcuts for PLC5 and SLC500 controllers.
- FactoryTalk LinxNetwork Browserversion 6.31.00 supports adding and configuring remote proxy drivers.
- FactoryTalk LinxNetwork Browserversion 6.31.00 enhances the configurations on theLLDPtab. The neighbor information also shows on thePort Configurationtab.
- FactoryTalk LinxNetwork Browserversion 6.31.00 adds audit messages for device configuration. When configuring device properties, audit messages are logged in the FactoryTalk Diagnostics Viewer.
FactoryTalk Linx version 6.40.00:
- FactoryTalk Linxversion 6.40.00 supports shortcut connections through a FactoryTalk Linx Gateway remote proxy server.
- FactoryTalk Linxversion 6.40.00 provides a 64-bit communications service for FactoryTalk Policy Manager.
- FactoryTalk Linxversion 6.40.00 updates the USB kernel drivers to permit Windows Core Isolation Device Security.
- FactoryTalk Linxversion 6.40.00 removes the 1784-PCICS card’s kernel driver.
- FactoryTalk Linxversion 6.40.00 supports FactoryTalk View ME Studio MER project file transfer to a VersaView6300 computer running FactoryTalk View ME.
- FactoryTalk Linxversion 6.40.00 supports switching the local language from a setting in the FactoryTalk Administration Console.
- FactoryTalk Linxversion 6.40.00 includes a new FactoryTalk Live Data Tag Browser that includes the ability browse Logix Extended Tag properties and bits embedded within integer tags.
- FactoryTalk Linxversion 6.40.00 supports REAL array and LREAL array data types for the CIA message.
- FactoryTalk Linxversion 6.40.00 supports Symbolic shortcut access to bits within Micro800 numeric tags.
- FactoryTalk Linxversion 6.40.00 increases the size of supported tag references received from FactoryTalk software from 260 characters to 1024 characters.
- FactoryTalk LinxNetwork Browserversion 6.40.00 supports the Explicit Protected Mode function.
- FactoryTalk LinxNetwork Browserversion 6.40.00 supports customizing the IP subnet with rotary switches on the controllers.
- FactoryTalk LinxNetwork Browserversion 6.40.00 adds a driver to communicate through a FactoryTalk Linx Gateway Remote Proxy service.
- FactoryTalk LinxNetwork Browserversion 6.40.00 adds an auto-start and minimize to the system tray option.
- FactoryTalk LinxNetwork Browserversion 6.40.00 supports uploading IODD device description files from an IO-Link device and registering them with the Device Description (formerly EDS) Subsystem.
- FactoryTalk LinxNetwork Browserversion 6.40.00 increases the number of items that can be added to the Ethernet driver list from 64 to 255.
- FactoryTalk LinxNetwork Browserversion 6.40.00 now displays the device's DNS host name in the topology tree along with its resulting IP address.
- FactoryTalk LinxConfiguration Import Export Toolversion 6.40.00 supports importing and exporting drivers without specifying a target server.
FactoryTalk Linx version 6.50.00:
- FactoryTalk Linxversion 6.50.00 supports automatically selecting an alternative network interface card (NIC) when the current one becomes unavailable.
- FactoryTalk Linxversion 6.50.00 supports the 1756-RM3 ControlLogix Redundancy Module (Redundancy Module Configuration Tool version 10.00.00 is required).
- FactoryTalk LinxNetwork Browserversion 6.50.00 supports discovering devices using LLDP table in EtherNet/IP in-cabinet networks.
- FactoryTalk LinxNetwork Browserversion 6.50.00 enhances the device locator function to support a wider range of devices, including the Stratix 5200 and 5800 industrial Ethernet switches and the 1783-ETAP3T module.
FactoryTalk Linx version 6.60.00:
- FactoryTalk Linxversion 6.60.00 supportsEtherNet/IPIn-cabinet Solution.
- FactoryTalk Linxversion 6.60.00 supports 1756ControlLogix®5590 Controllers.
- FactoryTalk Linxversion 6.60.00 supportsStratix™4100EtherNet/IPTest Access Point (ETAP).
- FactoryTalk Linxversion 6.60.00 supports tags fromFactoryTalk Design Studio®.
- FactoryTalk Linxversion 6.60.00 adds new predefined tags (@AlarmClass and @AlarmGroup) to show the value of alarm class and alarm group from a Logix controller.
- FactoryTalk Linxversion 6.60.00 supports a newFactoryTalk Linxextended tag property @Shortcut.
Provide Feedback