FactoryTalk Linx configurations adoption
Three types of
FactoryTalk View
applications can use FactoryTalk Linx
configurations:- Local stand-alone applications (created inFactoryTalk View SEorFactoryTalk Administration Console)
- Network (distributed) applications (created inFactoryTalk View SEDistributed)
- FactoryTalk View MEapplications
To begin using
FactoryTalk Linx
, you must first add it to a FactoryTalk
application, which is created in a FactoryTalk Directory
. This can be done within the FactoryTalk Administration Console
environment, or with FactoryTalk View SE
Standalone, FactoryTalk View SE
Distributed, or FactoryTalk View ME
products.FactoryTalk Linx
configurations can be edited in both FactoryTalk View Studio
and FactoryTalk Administration Console
. FactoryTalk Administration Console
is installed with FactoryTalk
Services.Although many of the steps to configure
FactoryTalk Linx
are shared between products, they have been grouped for clarity and convenience.Provide Feedback