FactoryTalk Linx configuration
A
FactoryTalk Linx
configuration consists of:- A list of communication devices and their settings, such as node and baud rate.
- Device drivers and their associated properties.
- A list of potential target devices with whichFactoryTalk Linxcan exchange data.
- Shortcuts. A shortcut is a name that represents the device you want to connect to, and the data that the device contains. The communication path associated with the shortcut tells the application where to find that data.
Provide Feedback