Read extended properties
Use extended properties to define additional information, such as engineering units, state identifiers, for components within your controller project in
Studio 5000 Logix Designer
version 21.00.00 or later. Once configured, the values of extended properties can be distributed to local and distributed clients, such as FactoryTalk View
version 9.00.00.Provide Feedback