Configure for local stand-alone applications
Use the procedure below to configure
FactoryTalk Linx
to work with your local (stand-alone) applications.To configure
FactoryTalk Linx
for local (stand-alone) applications:- Add aFactoryTalk Linxdata server to an application.
- Specify generalFactoryTalk Linxserver properties.
- (optional) ConfigureFactoryTalk Linxto supportFactoryTalk Alarms and Events.
- (optional) Register device description files in theDevice Description File Installation Tool.
- Add drivers and devices to your network or workstations, using the tabs on theCommunication Setupeditor. A driver is the software interface that allows you to communicate with your target hardware device.
- Create shortcuts that point to your target devices, or the devices from which you wish to collect data, using theCommunication Setupeditor.
- Close theCommunication Setupeditor, and outside ofFactoryTalk Linx, proceed to set up tags:
- If you are setting up an application in theFactoryTalk Administration Consoleenvironment, refer to theFactoryTalkAdministration Help.
- If you are usingFactoryTalk View SE, refer to theFactoryTalk View SEHelp.
TIP:
FactoryTalk Linx
runs as a service under the Windows LocalSystem account (that is, equivalent to Administrator).Provide Feedback