Data communication inhibit and enable
FactoryTalk Linx
enables you to control which shortcuts are active through both the FactoryTalk Admin Console and from an HMI screen. It provides appropriate system diagnostic indications that reflect that communications to the targeted device is intentionally inhibited. By doing this, the system loading time and network bandwidth needs could be reduced. The system usability could be improved as well by inhibiting and enabling data communication flexibly.Provide Feedback