DeviceNet Scanner Properties, General tab

How do I access this dialog box?
The
DeviceNet Scanner Properties
dialog box,
General
tab, automatically shows when you select the
DeviceNet Scanner
from the
Device Selection
dialog box.
You can also right-click the
DeviceNet Scanner
and then click
Properties
to display the dialog box.
Use the
General
tab of the
DeviceNet Scanner Properties
dialog box to:
  • View and adjust the name of the driver
  • Set the node address
  • Set the slot number in the virtual backplane
  • Set the baud rate
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal