DeviceNet Scanner Properties dialog box, General tab settings

The
General
tab of the
DeviceNet Scanner Properties
dialog box contains the following settings:
Setting
Description
Name
Used to view or adjust the device properties. The name can have up to 256 characters, and cannot contain a period, left bracket, or right bracket.
Node Address
Used to set the node address. Valid values are 0-63 and must be unique. You will receive an error message if the address entered is a duplicate or if it is out of range.
Slot in Virtual Backplane
Used to set the slot number in the virtual backplane. Valid values are 1-16.
Tip:
When a
PanelView
device loads a DeviceNet Scanner configuration, the virtual backplane slot number specified in the configuration is ignored. Instead, since there are only two slots in the
PanelView
Device's virtual backplane, with the
PanelView
system itself residing in slot 0, the DeviceNet Scanner is automatically assigned to slot 1.
Baud
Used to configure the baud rate for the driver that transmits data to your device. Available baud rates are 125,000; 250,000; and 500,000. The default is 125,000.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal