Configure DeviceNet I/O
Use this procedure to configure I/O on the DeviceNet Scanner. This is an overview of the required steps.
Prerequisites
- Before you configure, or define, the I/O in the DeviceNet Scanner usingFactoryTalk Linx, use theto insert connections and apply the scanlist to the network.Rockwell SoftwareScanlist Configuration Tool
To configure I/O on the DeviceNet Scanner
- Add aDeviceNet Scanner
- Add an address block
- Add a device to the address block
- Add an alias
After the I/O is configured, configure a device shortcut that references the DeviceNet I/O scanner. When you browse for tags exposed by this
FactoryTalk Linx
server, the aliases you configured will display.Provide Feedback