Virtual Backplane Properties dialog settings
The
Virtual Backplane Properties
dialog box contains the following information:Setting | Description |
---|---|
Auto Configure | Used to inform FactoryTalk Linx that it should automatically search for and insert it into the first available slot in the virtual backplane. Typically this setting should remain at the default state of not selected.If you are running a SoftLogix controller on the same computer as FactoryTalk Linx , you may need to clear this box and enter a specific slot for which FactoryTalk Linx should insert itself. This would be necessary to match a configuration that exists within the SoftLogix system.Tip: On a PanelView Plus device, the Virtual Backplane driver provides access to a ControlNet card or a DeviceNet card. |
Slot | This is the node address or the slot position of FactoryTalk Linx in the virtual backplane. On the PanelView Plus , the only valid slot position is 0, and this is the slot which will be used regardless of what is specified in the configuration. On the desktop, valid slot positions are 1 to 16 decimal. |
Provide Feedback