Virtual Backplane Properties dialog
How do I access the Virtual Backplane dialog box?
From the
Explorer
under the FactoryTalk Linx
data server, double-click Communication Setup
, right-click the configured Virtual Backplane driver and then click Properties
.Use the
Virtual Backplane Properties
dialog box to:- Enable Auto Configure
- View the slot position ofFactoryTalk Linx
Provide Feedback