RIO Properties dialog

How do I access the dialog?
From the Explorer under the
FactoryTalk Linx
data server, double-click
Communication Setup
, right-click the configured PKTX RIO driver and then click
Properties
.
Use the
General
tab on the
RIO (Remote I/O) Properties
dialog to:
  • Display or adjust the name of the 1784-PKTX or 27110-RN6 on a Remote I/O driver
  • Display the Jumper ID card number
  • Set the baud rate
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal