ControlNet Scanner Properties, General tab

How do I access this dialog box?
The
ControlNet Scanner Properties
dialog box,
General
tab, automatically shows when you select the ControlNet Scanner from the
Device Selection
dialog box.
You can also right-click the ControlNet Scanner, and select
Properties
to open the dialog box.
Use the
General
tab on the
ControlNet Scanner Properties
dialog box to:
  • Display or adjust the name of the device
  • Set the node address
  • Select the slot number for the virtual backplane
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal