Add a ControlNet scanner
In order to configure I/O on the ControlNet scanner in
FactoryTalk Linx
, the first step is to add a ControlNet scanner card in the Add Device
dialog box.To add a ControlNet scanner
- Right-click the virtual backplane (Communications tree,Communication Setupeditor) and then clickAdd Device.
- Select theControlNet Scanner card (1784-PKTCS)from theAdd Device Selectiondialog box to display theControlNet Scanner Propertiesdialog box,Generaltab.TIP:There can be only one ControlNet Scanner perPanelViewdevice.Note that this is the device to which you will configure a device shortcut. It is also important to note that youdo notneed a 1784-PKTCS installed on the workstation you are using to develop the ControlNet I/O configuration. In that case, you will be able to define a configuration but you will not be able to test the HMI application on the workstation.
- In theGeneraltab, enter theName. The default name is 1784-PKTCS ControlNet Scanner. The name can have up to 256 characters, and cannot contain a period, left bracket, or right bracket.
- In theGeneraltab, select theNode Address. Valid values are 1-99 and must be unique. You will receive an error message if the address entered is a duplicate or if it is out of range.
- In theGeneraltab, select a number in theSlot in Virtual Backplanefield. Valid values are 1-16. Refer toControlNet Scanner Properties, General tab settingsfor details on the Slot address.
- ClickOKto save the settings and close the dialog box.TIP:When aPanelViewdevice loads a ControlNet Scanner configuration, the virtual backplane slot number specified in the configuration is ignored. Instead, since there are only two slots in thePanelViewDevice's virtual backplane, with thePanelViewsystem itself residing in slot 0, the ControlNet Scanner is automatically assigned to slot 1.
Provide Feedback