- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create elements for controlling the min value
Create a label and a gauge to control the minimum value.
- Create the minimum value label:
- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the label, select, and enterMinValueLabel.
- InPropertiesand setTexttoMinimum Value.
- Create the min gauge:
- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the gauge, select, and enterMinGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
Provide Feedback