- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a complex dynamic link
Create complex dynamic links to transform linked values.
- InProject view, select an object that contains a property to link.
- InPropertieshover-over the property to link, select.Add Dynamic Link
- In the dynamic link browser, selectAdvanced.
- (optional) To open the complex dynamic link editor in the central pane, selectOpen in editor.TIP: Opening the complex dynamic link editor in the central pane is useful if you edit a complex dynamic link with a lengthy logic.
- To insert a dynamic link:
- Selectand selectInsertDynamic link.
- Set the dynamic link source by selectingor dragging and dropping an object or a property.Add Dynamic LinkThe reference to the selected node or variable appears in the property. Before the property,
appears to indicate that the property contains a dynamic link.
TIP: If the dynamic link does not resolve at design time,appears before the dynamic link. A dynamic link to a Windows alias may resolve at runtime. If the dynamic link is broken because the linked attribute no longer exists or has been moved,
appears before the link.
- To insert a converter:
- Selectand select a converter.Insert
- Create the converter logic by entering data or creating dynamic links in the converter fields.TIP: You can create a dynamic link by selectingor dragging and dropping an object or a property.Add Dynamic Link
- To change the dynamic link direction, select the icon:
Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.
- To link the source variable to the specific index of the parent variable:
- SelectConfigureand selectAdd parent array index.
- SetParent array index value.
- To create a converter on which you can dynamically build the variable source path, selectConfigureand selectEU Mode:
- Default. No conversion is applied.
- Localize. Sets the unit of measure of the parent variable based on the user locale.
- Copy EU from source. Sets the unit of measure of the parent variable as the unit of measure of the source variable.
- To add a dynamic path converter:
- SelectConfigureand selectKey-value converterorConditional converter.
- Set the converter properties.
- To delete a dynamic link or a converter, in the block, select.Delete
Provide Feedback