- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure a button to open a dialog box
To show a dialog box at runtime, another object must call a specific method.
Prerequisites
- Create a button. See Create a graphic object from a type.
- Create a dialog box type. See Create a graphic object type.
- To configure a button to open a dialog box
- InProject view, select a button object.
- InEvents, next toMouseClick event, selectand select .
- Create a dynamic link between theDialogargument and aDialog Box (type).For more information about dynamic links, see Create dynamic links.
Provide Feedback