- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create an event logger
Create a logger that monitors the current temperature.
- InProject view, right-clickLoggersand select .
- Configure events:
- InProperties, next toEvent configurations, select.
- SetListen subtreetoFalse.
- Set theEvent typetoAlarmConditionType.
- InProperties, double-clickEventLogger1
- In the central pane, select these variables:
- .
- .
- .
- .
- .
- .
- In the central pane, selectApply.
- Create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
Provide Feedback