- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
LogicObject.SetAlias(string, IUANode)
Sets the value of an alias, or the node the alias points to.
void SetAlias(stringaliasName, IUANodepointedNode);
Arguments
- aliasName(string)
- TheBrowseNameof the alias to set.
- pointedNode(IUANode)
- ANodeto which the alias must point to.
Example
The following example shows the
MotorInstance
alias that points to the Motor1
node.var myMotorInstance = Project.Current.FindObject("Motor1"); LogicObject.SetAlias("MotorInstance"), myMotorInstance);
Provide Feedback