- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a refresh button
Create a button that refreshes data in the data grid.
TIP:
Instead of creating this widget from scratch, you can add
Alarms Event Logger
from Template Libraries
that includes the refresh button.- InProject view, right-clickMainWindow (type)and select .
- InProperties, setTexttoRefresh Data.
- InEvents, next toMouseClick event, selectand select
Provide Feedback