- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Add a screen instance
Create an instance of a screen type and modify the screen instance properties.
Prerequisites
- Right-click a node to contain the screen object and select.The screen object instance appears under the node and inherits the properties of the screen type.
- (optional) InProperties, set the screen instance properties.For more information, hover-over the properties.
- (optional) Add objects to the screen instance.
Provide Feedback