- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create the System object
The
System
object allows users to view and configure certain system variables, such as the date and time, device, display, and application settings for the FTOptixApplication
.Create one
System
object per project.- InProject view, right-clickModeland then select .System1appears inProject view.
Provide Feedback