- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Manage dynamic links
Use C# APIs to set or remove dynamic links on the variables.
The APIs are supplied by the
IUAVariable
C# class.
TIP:
By default, dynamic links defined in a NetLogic are read-only, whereas dynamic links created with the
FactoryTalk Optix Studio
UI are read and write.Provide Feedback