- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Move an object
Move an object in the editor to position objects as they will appear at runtime. All of the objects in a container move with the container.
- To move an object
- In the editor, select and drag the object.
- InProject view, select the object and then inPropertieschange:
- Horizontal alignment. Enter the value for the space between the object and the X-axis.
- Vertical alignment.Enter the value for the space between the object and the Y-axis.
TIP: The position of the object inProject viewdetermines the order of objects on the Z-axis compared to other objects in the same container. Objects lower in the tree appear higher in the order on the Z-axis.
Provide Feedback