- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Resize an object
Drag to resize an object or specify values in object properties.
Prerequisites
To resize an object, the alignment of the object must be left, top, or bottom. If the object alignment on the X-axis or Y-axis is
Adjust
, the object sizes dynamically according to the size of the container. You cannot scale the size of an object that is inside a container with respect to the size of the container.
TIP:
The size of the
Window
object defines the size of the entire user interface. It can be set using the Width
and Height
properties or it can be automatically set equal to the size of the screen on which the interface is displayed at runtime using the Full Screen
property.- To resize an object
- In the editor, drag a sizing handle on the object.
- InProject view, select an object and inPropertieschange:
- Height. Enter the value for the height of the object.
- Width. Enter the value for the width of the object.
TIP: If you delete either theHeightorWidthvalue, the object uses theAutosetting. Text determine the size of the object.
Provide Feedback