- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
PDF Viewer
Displays a PDF file at runtime.
Operation
The PDF viewer can display either:
- A local PDF file stored in the project directory
- A PDF file stored on a remote serverPDF viewer supports these protocols for displaying remote PDF files:
- http
- https
Use case
Use embedded PDFs to provide the end users with quick access to technical documentation.
Provide Feedback