- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Add an address bar
Add an address bar for the
Web browser
object.
TIP:
The address that you enter must start with the protocol. For example,
https://rockwellautomation.com
Prerequisites
- To add an address bar
- InProject view, create aWeb Browserobject.
- Create anEditable Labelobject.
- Create variable of String data type.For more information, see Variables.
- (optional) Determine the start page by entering a web address as the variable value.For example, enterhttps://www.rockwellautomation.com
- Create a dynamic link between theTextproperty of theEditable Labelobject and the variable.For more information about dynamic links, see Create dynamic links.
- Create a dynamic link between theURLproperty of theWeb Browserobject andEditable LabelTextproperty.For more information about dynamic links, see Create dynamic links.
Provide Feedback