- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Integrate the interface with the NetLogics
Integrate the NetLogics with the application interface.
- InProject view, expand .
- Configure the Insert Random Data button:
- InProject view, selectInsertButton.
- InEvents, next toMouseClick event, selectand select .
- Configure the Display Query in Label button:
- InProject view, selectRunQueryButton.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback