- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure a button to close a dialog box
To hide a dialog box at runtime, another object must call a specific method.
Prerequisites
Create a dialog box type. See Create a graphic object type.
- To configure a button to close a dialog box
- Create a button object as a child of the dialog box type.For more information, see Create a graphic object from a type.
- InEvents, next toMouseClick event, selectand select theClosemethod.
Provide Feedback