- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Dock an object
Anchor objects in the container by docking the object.
Dock objects on any side of the container while maintaining margins, in the center while resetting margins, or stretch objects across a container.
- InProject view, double-click a container or select.The editor opens in a separate tab.
- In the editor, select the objects to dock.TIP: To select multiple objects, hold downCtrland select multiple objects.
- In the editor toolbar, select the button to dock the object:
- Dock left. Anchor the selected objects the left while maintaining margins.
- Dock right. Anchor the selected objects on the right while maintaining margins.
- Dock top. Anchor the selected objects at the top while maintaining margins.
- Dock bottom. Anchor the selected objects at the bottom while maintaining margins.
- Dock center. Anchor the selected objects vertically while centering the objects and resetting margins.
- Dock center. Anchor the selected objects horizontally while centering the objects and resetting margins.
- Dock left and right. Stretch the selected objects horizontally across the container.
- Dock top and bottom. Stretch the selected objects vertically across the container.
Provide Feedback