- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Implement the UIPopulator NetLogic
Point the NetLogic to the graphic objects.
- InProject view, selectUIPopulator.
- InProperties, at the top, selectand selectVariable.
- Hover-over the variable, select, and enterModelObject.
- Next toModelObject, selectInt32and selectNodeId.TIP: If you do not see the required option, select theShow allcheckbox.
- Create a dynamic link betweenModelObjectand .
Provide Feedback