- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Read operation codes
For each reading operation of single or multiple tags, the controller generates an operation code that describes the operation result.
Code | Description |
---|---|
Good | The reading operation is successful |
BadNoCommunication | The reading operation failed because of a timeout (for example, a connection timeout). The timeout value is determined by the Timeout property of a Communication station object. |
BadCommunicationError | The reading operation failed because the controller returned an error |
BadConfigurationError | The reading operation failed because of a tag configuration error (for example, an invalid address) |
Provide Feedback