Configure controllers

Right-click any controller branch in the
Preview
or
Class View
pane to view the controller configuration commands.
This table describes each
Controller
command. Commands appear at the applicable level of the tree.
Command
Description
Controller
Generate Controller
Generates a copy of the selected controller from ACM. Displays the
Logix Code Generation
dialog. Generates code (for example, L5X or ACD) for the selected controller.
Add New
Adds a controller object to the project using the
Object Configuration Wizard
.
Add New from ACD/L5X
Adds a controller object to the project from an ACD or L5X file. Additional objects may also be added depending on what is configured and available in the ACD file.
Update from ACD/L5X
Updates the ACM project based on an existing ACD file.
Detach from ACD/L5X
Removes the link between the ACM project and the attached ACD or L5X file.
Merge Controller
Merges content between the original ACM project, updated ACM project, and existing ACD or L5X file. Uses the Logix Designer Compare Tool.
Add New Program
Adds a program to the current controller object using the
Object Configuration Wizard
.
Add New Task
Adds a task to the current controller object using the
Object Configuration Wizard
.
Paste
Pastes the contents of the clipboard to the selected controller.
Paste Special
Pastes the contents of the clipboard to the selected controller with options.
Generate Partial Program
Displays the
Logix Code Generation
dialog. Generates a partial program for the selected task.
Generate Partial Routine
Displays the
Logix Code Generation
dialog. Generates a partial routine for the selected task.
Move Up
Moves the highlighted object up the tree.
Move Down
Moves the highlighted object down the tree.
Set Main Routine
This command is available when multiple main routines have been added from different library objects. There can only be one main routine. If a main routine is already selected, this command is dimmed.
Set Routine Instance Order
Displays the
Instance Execution Order
dialog that specifies the order in which any contributing objects insert their code into the routines.
Object
Import
Starts Import Export Manager.
Export
Starts Import Export Manager.
Delete
Deletes the selected object.
Copy
Copies the selected object to the clipboard.
Rename
Renames the selected object.
Update
Updates the selected libraries to the most recent version.
View
Project Library Usage per Library
Displays a report showing the registered library usage for the selected library. Available only at a library branch.
Network Layout
Generates
Network Layout
report.
Module I/O Schedule for Rack Module
Displays the
I/O Schedule
showing rack assignments.
Chassis Layout
Displays or prints a report with the I/O Modules in the Controller (local) chassis. Pastes the contents of the clipboard to the selected Controller with options.
Add New Instance
Adds a task in the
Class View
pane.
Navigate to Library
Navigates to the library in the
Registered Libraries
tree.
Object References
Displays the Object References report.
Exclude AOI (Add On Instructions)
Excludes the AOI (included by default). Only available in the
Add-On Instructions
branch.
When two AOIs with the same major and minor revision, but different extended texts are added in the
Preview
tree, the AOI conflict shows. You can use
Exclude AOI
to select which one to use.
Include AOI (Add On Instructions)
Includes the AOI. Only available in the
Add-On Instructions
branch.
Refresh
Refreshes the tree view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal