Add an instance
Use
Add New Instance
to add a library object instance to an existing library class
in the Class View
pane.To add an instance
- In theClass Viewpane, right-click the library class from which the new instance will be created and then clickAdd New Instance.TheObject Configuration Wizardis displayed.
- (optional) InName, enter a name for this instance.
- (optional) InDescription, enter identifying information about this instance.
- Configure the associated Task and Program.
- ClickFinish.
Provide Feedback