Add a controller from an ACD or L5X file
Add controllers to the
Application Code Manager
project from an existing Logix Designer XML file (.L5X) or Logix Designer Project file (.ACD).To add a controller from an ACD or L5X file
- In thePrevieworClass Viewpane, right-click theControllerfolder and then clickAdd New from ACD/L5X.
- In theSelect an ACD/L5X Filedialog, select the file to add then clickOpen.
- In theImport From ACD Wizard - Instance Import Actionspage, review the items listed. Items withAddin theActioncolumn are imported.
- If any objects should not be imported, clickAddand then selectExclude.
- SelectNext. TheImportdialog displays. The information grid shows any errors, warning, info, or debug messages generated during the import. Review any warnings or errors listed.
- ClickView Changesto see a comparison of the original and updated information in an Excel spreadsheet.
- Information buttons show how many of each type of message are present. Filter the displayed messages by clicking the button for the message type to toggle the display of those messages.
- SelectNext. TheImport From ACD Wizard - Content Importedpage displays.
- SelectFinish.The new object will appear in thePreviewpane andClass Viewpane.
Provide Feedback