Add a software object

Add reusable code for software objects (tasks, routines and programs) to the controller from the
Application Code Manager
library.
To add a software object to a controller
  1. Use one of the following methods:
    • In
      Preview
      , expand
      Controllers
      , expand the controller object, right-click a task or program object, then click
      Add New
      .
    • In
      Class View
      , expand
      Controllers
      , right-click the controller object, then click
      Add New
      .
  2. In the
    Object Configuration Wizard
    , expand the library categories to display the software libraries registered in the ACM database.
  3. Select the library object to add to the selected task or program, then select
    Next
    .
  4. (optional) In
    Description
    , type a unique description of the software or accept the default description.
  5. (optional) Edit software object parameters and fields in the tabs on the bottom half of the Object Configuration Wizard.
  6. (optional) If the software object depends on other linked library objects, select the
    Linked Libraries
    tab, then select Auto Create Linked Objects. Select linked library creation options, then click
    OK
    .
  7. Select
    Finish
    .
    The software object appears in the
    Preview
    and
    Class View
    panes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal