Auto Create Linked Objects
How do I open Auto Create Linked Objects?
- Use either of the two methods:
- InPreview, expandControllers, expand the controller object, right-click a task or program object, then clickAdd New.
- InClass View, expandControllers, right-click a controller project, then clickAdd New.
- In theObject Configuration Wizard, expand the library categories to display the software libraries registered in the ACM database.
- Select the library object to add to the selected task or program, then selectNext.
- If the software object depends on other linked library objects, select theLinked Librariestab, then selectAuto Create Linked Objects.
Use
Auto Create Linked Objects
to add objects linked by a library object to a project, rather than manually adding them to the project one at a time.Hardware modules cannot be Auto Created but can still be linked to if they exist in the
project.
Column | Description |
|---|---|
Link Name | Displays the name of the link in the object being added to the project. Auto Create Linked Objects uses the link name to find a matching library. |
Library | Displays the name and version of a library that matches the link name. The latest version of the library is always used if the version was not specified. If an exact library match cannot be found, the Library column displays "No unique library matches link criteria". The Action field is locked to Ignore . |
Action | Sets the action that Auto Create Linked Objects should take for the linked library:
Select multiple linked objects and use the action list to set the action to these objects. |
Object Name | Browse for an existing object name or set the auto created library object name. Disabled if the library object is parameterized. When an exact match library is found, the match icon displays beside the object name. |
Task Name | Assigns the auto-created library object to a task. Create a task by selecting
< Add New... >. Disabled if Action is set to Use
Existing or Ignore .Select multiple auto-created library objects and use the task name list to assign
these objects to one task. |
Program Name | Assigns the auto-created library object to a program. Create a program by
selecting < Add New... >. Disabled if Action is set to Use
Existing or Ignore .Select multiple auto-created library objects and use the program name list to
assign these objects to one program. The program name list is disabled if these
objects are unassigned. |
Provide Feedback