Object Configuration Wizard
How do I open the
Object Configuration Wizard?
Use either of the two methods:
- InPreview, right-click a folder, task, program, or I/O configuration node in the project, then selectAdd New,Add New Task, orAdd New Program.
- InClass View, right-click the project, controller, or library, then selectAdd NeworAdd New Instance.
Use the
Object Configuration Wizard
to add a library object, program, or task to a project. The Object Configuration Wizard
consists of two pages, the Select a Library
page and the Parameters
page.- TheSelect a Librarypage displays the latest revisions of library objects, grouped by category. SelectShow All Revisionsto display all revisions. To search for a library quickly, enter the criteria inFilter.
- TheParameterspage displays the name, description, and configuration parameters for a library object, program, or task. Parameters may be broken up into object-specific tabs, such as SubObjects, Linked Libraries, or Interface Links. Editable fields appear black, non-editable fields appear gray.TIP:If a library object contains links to other linked library objects, these objects can be created automatically. Select theLinked Librariestab (if applicable), then select Auto Create Linked Objects.
Provide Feedback