Generate a controller file
After configuring a controller in
Application Code Manager
, generate the Logix Designer files for the controller.To generate a controller file
- In thePrevieworClass Viewpane, right-click the Controller folder or the controller object and then clickGenerate Controllers.
- In theLogix Code Generationdialog, select theGenerateandACM Project Datacheckboxes.
- Select theOverwrite Existingcheckbox to replace an earlier controller file with the same name.
- SelectCreate ACDto create a Logix Designer Project file (.ACD) in addition to the Logix Designer XML file (.L5X).IMPORTANT:Generating controller files withACM Project Dataselected produces the most complete record of the controller data. Always selectACM Project Datawhen generating a controller file as part of a disaster recovery backup.If there is not a matching Studio 5000 Logix Designer version installed and theSoftwareRevisionis selected, theCreate ACDcheckbox is disabled.
- InSave Path, type the path where the controller files should be saved or use the default path:C:\Users\<username>\AppData\Local\Rockwell Automation\Application Code Manager\OutputReplace the <username> variable your current Windows username.
- ClickGenerate.The controller files are generated. A status message displays when completed.
- (optional) ClickOpen Folderto open the file explorer to the controller file location.
Provide Feedback