Contribute instances
Use the
Contributing instances
menu to view and edit the properties of an object
instance.To contribute an instance
- In thePreviewpane, expandControllers.
- Right-click a node shared by multiple instances, and then selectContributing instances.A list of contributing instances is shown.
- Select an instance.Its parameters property panel opens.
Provide Feedback