Select Destination Project dialog
The following table shows the options in the
Select Destination Project
dialog.Options | Descriptions |
|---|---|
Name | Displays the name of the destination project. |
Description | Displays the description of the destination project. |
New | Opens the Object Configuration Wizard dialog to create a project. |
OK | Starts the copying or moving process. |
Cancel | Returns the home page. |
Provide Feedback