Add a hardware module
Add hardware modules to your controller configuration in the
I/O Configuration
branch in the Preview
pane.To add a hardware module
- In thePreviewpane, expand theControllersnode, expand the controller object, expand theI/O Configurationfolder and then right-clickBackplaneand then clickAdd New.TheObject Configuration Wizarddisplays.
- Click the + symbol to expand the library category and display the hardware module libraries registered in the connected ACM database.
- Select the library that will be copied to create the hardware module and clickNext.
- (optional) InDescription, type a unique description of the hardware module or accept the default description.
- ClickFinish.The hardware module object appears in thePreviewpane underBackplane.
Provide Feedback