Add a controller

Use the
Object Configuration Wizard
to add a controller from a predefined controller library that resides in the registered libraries, configure its parameters, and include it in the ACM design output.
TIP:
The ability to add multiple controllers to a project or open an existing project containing multiple controllers is only available if the product has a Standard activation license and is not available in Lite mode.
To add a controller
  1. In the
    Preview
    or
    Class View
    pane, right-click the
    Controllers
    folder and then click
    Add New
    .
    The
    Object Configuration Wizard
    displays. Controller objects display in category groups. A triangular marker next to the column name denotes the current category grouping displayed. Change category groups by clicking a column heading.
  2. Click the + symbol to expand a category and display the controllers in that group.
    Controllers registered in the connected ACM database are listed.
  3. Click the desired controller, and then click
    Next
    .
  4. In
    Name
    , enter a name for the controller.
  5. (optional) In
    Description
    , modify the descriptive text as needed to help identify the controller.
  6. In the
    Parameters
    tab, adjust
    Controller
    ,
    HMI
    ,
    Historian
    , and
    Motion
    parameters as needed.
  7. Click
    Finish
    .
    The controller adds to the
    Preview
    and
    Class View
    trees.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal