Move or copy a controller
For projects in the same database,
Copy To
and Move To
allow you to copy or move a controller from one project to another project from the Class View
pane.
TIP:
This feature is only available if the product has a Standard activation license and is not available in Lite mode.
To move or copy a controller to another project
- In theClass Viewpane, expandControllers.
- Right-click the controller that will be copied or moved to another project.
- SelectCopy To.When selectingCopy To, the controller will be copied and pasted to the destination project.
- SelectMove To.When selectingMove To, the controller will be cut and pasted to the destination project. When the controller has unresolvable references, they will be cleared.
- In Select Destination Project, select an existing project or create a project as the destination project.When there is a name conflict between the moved controller and the controller in the existing project, rename the destination controller inRename Destination Controller.
- ClickOK.
- When prompted, selectOK.
- Once theLog File Vieweropens, track the errors, warning, informational, and debug events.
Provide Feedback