Merge controllers

Use
Merge Controller
to add or update objects from an ACM project into the attached ACD file.
To merge controllers
  1. In either the
    Class View
    or
    Preview
    pane right-click the object to merge.
  2. Select
    Merge Controller
    . The
    Logix Designer Compare Tool
    will be launched.
    Refer to the Logix Designer Compare Tool help files for further information.
    TIP:
    After the merge file has been created, confirm that all information is correct before deploying.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal