Update a controller
Update controller configurations in an
Application Code Manager
project using information from a Logix Designer XML file (.L5X) or a Logix Designer Project file (.ACD).To update a controller using an ACD/L5X file
- In thePrevieworClass Viewpane right-click the controller to update and selectUpdate from ACD/L5X.
- InSelect an ACD/L5X File, choose the ACD or L5X file to use to update the controller.TheImport from ACD Wizard - Instance Import Actionspage displays.
- Objects that are present in the file but not in the target controller will be selected to be added by default. If any of these objects should not be added selectExcludefrom theActioncolumn.
- Objects that exist in the target controller will default to being excluded from the update. If any of these objects should be updated using the information in the file selectUpdatefrom theActioncolumn.TIP:When excluding an object, information in the ACM project is preserved. When an update is performed, information from the ACD or L5X overwrites the ACM project information.
- SelectNext. The import operation proceeds. After the operation is finished theImport Completepage displays. The information grid shows any error, warning, info, or debug messages generated during the import. Review anyWarningsorErrorslisted.
- ClickView Changesto see a comparison of the original and updated information in an Excel spreadsheet.
- Information buttons show how many of each type of message are present. Filter the displayed messages by clicking the button for the message type to toggle the display of those messages.
- SelectFinish. TheImport From ACD Wizard - Content Importeddialog appears. If one or more objects are set to update, thenUpdate the Original Snapshotwill be checked by default. Clear the checkbox to prevent the snapshot information from updating the current configuration and then clickFinishto close the wizard.TIP:Snapshot information is used for the original ACM project data when performing the merge.If all items are excluded, by defaultUpdate the Original Snapshotis not checked.
- IfUpdate the Original Snapshotwas selected, clickNext. TheImport From ACD Wizard - Original Snapshot Updatedconfirmation page displays, clickFinishto close the wizard.
Provide Feedback