Delete a hardware module
If a module is no longer relevant to the application, it can be deleted from the project.
To delete a module
- In theClass Viewpane, right-click the module and then selectDelete.
- In theDeletedialog, clickYesto confirm that the module should be deleted.
- If other objects reference the object, theDelete Actiondialog displays.
- ClickClearto remove all references to the module being deleted.
- ClickOKto delete the module.The module is removed from theClass ViewandPreviewpanes.
Provide Feedback